Increasing Automotive Safety Through Embedded Radar Technologies
By Freescale
Featured Supplier
Featured Product
Related Resources
Introduction
There is a global trend in the increasing numbers of road fatalities. In 2010, 1.24 million people were killed on
the world’s roads, the eighth leading cause of death globally (World Health Organization). Within the developed
regions, passive car safety systems, seat belts, airbags, and crumple zones have proven essential in decreasing
fatalities and serious injuries to the occupants of cars and pedestrians.
Even within the developed regions of the world—where vehicles are becoming more connected and providing an
increasing level of information to the vehicle’s operator—analysts recognize driver distraction as a real
potential source for fatalities and serious injury. The demand for improving automated safety systems exists and
is increasing year-to-year.
While the global automotive industry strives for a goal of zero vehicle-related fatalities, and consumer demand
and government legislation drive improved automotive safety standards, the adoption of active and predictive
crash avoidance safety systems has become more prevalent in modern vehicles.
Proliferation of Advanced Driver Assistance Systems (ADAS)—such as electronic stability control and rear-view
facing cameras, and vision-based pedestrian detection systems—has been possible due to improvements in MCU and
sensor technologies. Enhanced radar-based embedded solutions offer complementary safety features to ADAS
designers.
Increasing Use of Radar-Based Safety Systems
As more advanced ADAS systems are expected to become government-mandated in the future following the recent
introduction of legislation such as rear-view facing cameras in vehicles and advanced emergency brake assist
(AEBA) for commercial vehicles, Freescale has developed new products to support these much-needed applications.
Radar-based safety systems manage blind spot and side-impact detection, as well as long-range and mid-range
frontal radar for adaptive cruise control. Freescale is the market leader in embedded radar solutions and has a
highly skilled design team driving new innovations in embedded MCUs and 77 GHz millimeter wave integrated
circuits specifically tailored for radar applications.
A typical radar module consists of a transmit solution (Tx), a voltage-controlled oscillator (VCO), and a
three-channel receiver IC (Rx), along with a MCU. The chips are connected via the local oscillator (LO) signal,
around 38 GHz. The individual control of each chip is implemented by a serial peripheral interface (SPI) bus.
The main controller and modulation master is a single MCU with integrated high- speed analog-to-digital
converters (ADCs) and appropriate signal processing capability, such as Fast Fourier Transforms (FFTs).
Freescale introduced the next-generation of embedded radar-based products with the Qorivva MPC577xK MCU and the
MR2001 77 GHz radar transceiver chipset. The radar transceiver chipset consists of a VCO (MR2001VC), a
two-channel Tx transmitter (MR2001TX), and a three-channel Rx receiver (MR2001RX). These new products deliver a
complete embedded radar system for automotive designs.
These state-of-the-art radar solutions complement Freescale’s existing arsenal of high-performance ADAS
solutions. For example, Freescale’s embedded camera/video offerings—such as the SCP220x image cognition
processor (ICP) family and the Qorivva MPC5604E MCU—are designed for advanced vision processing to address
object detection from vehicle to pedestrians. With the release of the new radar-based products, Freescale now
offers a comprehensive ADAS solution for automotive manufacturers’ requirements.
This white paper will address the benefits of the MPC577xK MCU from both a technical and bill of materials (BOM)
optimization perspective.
The Qorivva MPC577xK MCU: Industry-Leading Integration and Performance
Many current radar systems are based around the Qorivva MPC5675K MCU—, including external FPGA, ADC, DAC, SRAM,
and analog front-end for transmitting and receiving. The MPC577xK MCU is specially designed to enable a
cost-effective radar system with increased performance in a single chip solution.
The MPC577xK family attains its cost-advantage by providing high levels of digital and analog integration within
a single 356 BGA package and removes the requirement of having an external FPGA, ADC, DAC and SRAM, thereby
reducing the number of components required, the PCB size, and the complexity of software (Figure 1).
Figure 1: Radar Chipset Evolution
In addition to the two 266 MHz e200z7 processing cores, the MPC577xK MCU also features a state-of-the-art signal
processing toolbox (SPT). This contains the hardware modules required for processing sampled signals from short,
medium and long-range radar applications. The SPT is a powerful processing engine containing high-performance
signal processing operations driven by a specific instruction set. Its programmability ensures flexibility while
removing the CPU from frequent scheduling of hardware operations, while still controlling and interacting with
the processing flow.
- Highly integrated MCU reduces the total number of components required, the size of the PCB, and the
complexity of the software
- Easy-to-use MCU with integrated FFT accelerator
- Large-density memories to support scalable radar applications
- Supports open-loop and phase-locked looped systems, enabling design flexibility
- Contained power dissipation improves efficiency
- Helps system manufacturers meet the functional safety ISO 26262 ASIL-D target
Figure 2: Qorivva MPC577xK MCU Block Diagram
The MR2001 77 GHz Radar Transceiver Chipset: High Performance and Scalable to Multi-Channel
The MR2001 77 GHz radar transceiver chipset is an expandable, high-performance,three-package solution for
automotive radar modules. The chipset consists of a VCO, a two- channel Tx transmitter, and a three-channel Rx
receiver. These three parts are each packaged in a 6 mm x 6 mm fan-out wafer-level package on a 500 µm pitch.
This package technology is ideal for 77 GHz radar applications since it provides extremely low insertion loss and
parasitics at frequencies up to 100 GHz. The packaged chipset simplifies the end user’s assembly of the radar
module since there is no need for chip and wire assembly techniques for bare die. Furthermore, the chipset
readily scales up to four Tx channels and 12 Rx channels, enabling a single radar platform capable of electronic
beam steering across a wide field-of-view and supporting long-, mid-, and short-range radar applications over a
full selection of vehicles—from budget to luxury.
- Scalable to two Tx channels and 12 Rx channels with simultaneous active channels to enable a single platform
capable of electronic beam steering across a wide field-of-view
- Advanced packaging technology to ensure the highest performance and minimum signal interference on the
customer PCB
- Low power consumption—2.5 W typical for the complete transceiver
- Supports fast modulation at 100 MHz/100ns
- Best phase noise performance < -93="" dbc/hz="" at="" 1="" mhz,="" offset="" to="" improve="" target="">
- Integrated baseband filter and VGA saves system BOM cost
- Local oscillator at 38 GHz to lower the distribution loss and reduce system interference
- Bi-phase modulator on the transmitter chip supports rejection of parasitic signals
Figure 3: MP2001 77 GHz Packaged Radar Chipset
Advanced Packaging Technology
The MR2001 radar transceiver chipset is designed with advanced packaging technology that delivers excellent
thermal and electrical performance. The package is qualified to support rigorous automotive standards including
solder joint reliability, deep temperature and humidity cycling, and EMC performance. The packaging technology
is available for leading suppliers and is compatible with reduction of hazardous substances (RoHS) standards.
Open-Loop Radar
The MPC577xK MCU and the MR2001 77 GHz packaged radar transceiver chipset are designed to support an open-loop
radar system. In such systems, a phase-locked loop is not required to generate linear chirps (FMCW modulation).
This approach lowers the total system power consumption.
The open-loop concept is typically used in combination with a fast chirp FMCW modulation with a chirp time in the
range from 10 µs to 100 µs. Fast chirp systems lower the duty-cycle and improve the SNR of a radar system
because a full radar image is captured quicker. The potential disadvantage of high-baseband frequencies is that
they drive higher analog bandwidth andsampling rates of the required ADC. The MPC577xK MCU overcomes this
potential problem since it has integrated up to 8 ∑Δ-ADC with 5 MHz bandwidth and an internal sampling clock of
320 MHz.
In an open-loop radar system, the MCU is the chirp master with a digital-to-analog converter (DAC) providing the
tuning voltage for the VCO. Depending on the tuning voltage, the VCO generates a high-frequency signal (LO),
which then drives the different receiver and transmitter chip.
During normal operation, linear frequency chirps are transmitted and reflected signals are received. The
receivers in combination with the transmitter are arranged as homodyne system so that the received signals are
down-converted directly into the baseband. Such baseband signals are thenfiltered and amplified (filters and
variable gain amplifiers are implemented in the receiver chips) and differentially feed to the ∑Δ-ADC of the
MPC577xK MCU. By converting the baseband signals into the digital domain, following the digital beam forming
approach, applying FFTs and tracking algorithms, objects can be identified in terms of distance, velocity, and
angular position.
Radar Application
The MPC577xK MCU is suitable for radar applications that may require up to eight antennas each, acquiring up to
2048 possible samples simultaneously, which are then converted by a 12-bit ΣΔ-ADC at a sample rate of up to 10M
samples-per-second-per-chirp. This can be achieved through Freescale’s new 8-channel ADC architecture in
conjunction with flexible/programmable decimation filtering and inherent anti-alias filtering. It’s also
designed with excellent immunity to substrate noise and complete isolation from the rest of the MCU’s
peripherals, while still meeting low-power targets designed for low-power applications.
Figure 4: Radar Applications
Once a measurement cycle consisting of possibly 256 chirps is acquired, this data is thenpre-processed using the
on-chip data acquisition block and grouped according to the antennas. It’s then transferred to the system SRAM
using the sample direct memory access (DMA). The data acquisition module receives samples from the SDADC,
extracts the samples in the acquisition window.
After all the data for a chirp is acquired, the data is transferred to the SPT’s local SRAM using the
programmable DMA engine and frequency transformed using the new embedded FFT engine. The hardware accelerated
FFT module can perform complex and real FFTs with a configurable length and can also execute a windowing
operation which can be calculated with the data.
The FFT is capable of 16/24-bit integer FFTs of up to 4K points and 2x real by complex. For further signal
processing, the data can be transferred to the system SRAM or directly to the CPU tightly coupled memories (TCM)
where it can be processed by the e200z7 cores utilizing the SPE2 (a 16-bit four-way SIMD integer unit) or the
VFPU (two-way SIMD single-precision FPU).
The command sequencer executes a sequence of commands required for processing the radar data, and in conjunction
with the new cross timing engine (CTE), defines the individual timing of signals for the radar system and
controls the complete radar processing flow, including the analog front end (AFE). The integration of the new
high-performance AFE also includes a new best-in-class 12-bit resolution DAC which has a maximum of 2 Ms/s. In
the radar system, the DAC converts the chirp waveform to an analog signal that controls an external VCO for
voltage-to-frequency conversion.
Embedded Radar Components
The SPT (as seen in Figure 3) consists of:
Acquisition Block
- Channel muxing—Sample re-ordering to simplify PCB routing
- Sample DMA—Merging ADC samples into memory words, arranging the data into packets, and distributing to
memory locations
Programmable DMA (PDMA)
- Transfers data between the system RAM/Flash/TCM to operand RAM or twiddle RAM (SPT internal RAMs) and
vice-versa
- Performs special packing and unpacking schemes on the fly, for reduced storage
Memory
- Operand RAM stores the operands for operations like FFTs
- Twiddle RAM stores constants like coefficients used in FFT operations
- Work registers store single values for calculation (such as coefficients)
Hardware Accelerator
- FFT
- Radix4 and Radix2 butterfly and twiddle multiplication
- Windowing for pre- and post-multiplication with coefficients
- Copy
- Primarily moves data from one location to another
- Can transpose and pack complex data and manipulate real/imaginary parts
Command Sequencer
- The command sequencer reads and interprets instructions in the command queue and triggers the
operation specific scheduler depending on the instruction
These newly integrated, high-performance radar HW modules are also supported by communication interfaces
for off-chip communication:
- FlexRay: Up to 20Mb/s dual-channel data to other controllers (e.g., object information, active/
passive safety relevant data)
- DSPI/IIC/LIN: E.g., setup/status information from the front-end ASIC
- CAN/CAN-FD: Up to 3Mb/s arbitrary data to other car components
- Ethernet: 100Mb/s data
- LFAST: Inter-processor communication (IPC) data to other tightly coupled MCUs for the radar
processing system
As part of the Freescale SafeAssure program, the MCP577xK MCU has been designed with two high-
performance e200z7 cores—based on Power Architecture® technology—for signal processing and can
help car manufacturers achieve a minimum ISO 26262 Automotive Safety Integrity Level-B (ASIL-B). In
addition to supporting the requirements of automotive functional safety applications, there are two
e200z4 cores in a lockstep configuration specifically designed for decision-making and safety-critical
requirements, helping to achieve ISO 26262 ASIL-D certification.
Some additional key safety features include online logic built-in self-test (LBIST) and memory built-in
self-test (MBIST), end-to-end error-correcting code (ECC), clock and power generation supervisor, and a
failure-handling module—which also enable customers to obtain ASIL-D certification.
Conclusion
The increasing global need for active and predictive safety systems in mainstream vehicles is driving the
need for semiconductor suppliers to deliver new innovations. These solutions must enable system
suppliers and OEMS to optimize the bills of materials of current radar systems in terms of not only cost
but also footprint. Manufacturers are further incorporating radar for blind spot and side-impact
detection, in addition to long-range and mid-range frontal radar.
As a market leader in embedded radar systems, Freescale’s newest radar-based solutions present unique
capabilities for designers of next-generation ADAS systems—enabling them to not only comply with the
latest regulatory standards, but also (and best of all) save lives.