Mouser Electronics - Distribuidor de componentes electrónicos
 
Costa Rica - Marcar Costa Rica

Términos internacionales de comercio (Incoterms):FCA (punto de envío)
Los costos de aranceles, aduana e impuestos se cobrarán en el momento de la entrega.

Confirme su elección de moneda:

Colón costarricense
Solo se aceptan pagos con tarjetas de crédito, excepto American Express

Dólares estadounidenses
Se encuentran disponibles todas las opciones de pago

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: 3 Connectors That Keep the Current Safely Flowing Tommy Cummings

New Tech Tuesday

Join journalist Tommy Cummings for a weekly look at all things interesting, new, and noteworthy for design engineers.

Design engineers are well aware of the rapid advancements in connector and component designs. To simply connect electrical conductors and create an electrical circuit, developers must continually deal with thousands of configurations with different power-handling capabilities.

All the while, developers are creating more challenging form-and-fit parameters while providing as much or increasing functionality as older connectors.

To pile on even more, you've got an accelerated electric vehicle and plug-in hybrid industry and its power infrastructure added to the mix.

This is why designers of connectors rarely leave the workbench—lots to design.

To address the simple diversity of connectors, this week's New Tech Tuesdays examines three different types of connectors and what project developers can optimize them for connection solutions.

 

EVs, Battery Storage, and Pluggables Need to Connect

Phoenix Contact E-Mobility CHARX Charge Inlets are ideal for EV battery charging and plug-in hybrid vehicle charging design. These connectors allow high-power charging up to 250A continuous and up to 500A on a temporary basis. CHARX inlets are versatile. They can be developed for charging standards in different regions and for Type 1 and Type 2 variants. The inlets' dimensions and mounting features are identical, giving designers the same assembly space in the vehicle.  

HARTING Han® S Modular Battery Storage Connectors provide secure connection technology for modular battery storage systems. The sustainable use of renewable energies, such as wind or solar, can be achieved through energy storage modules because they enable time-delayed, needs-based use. HARTING connectors can accelerate the buildup of energy storage modules using lithium-ion cells. The connectors have compact and flexible lockable hoods and housings that provide space for connections with a capacity of up to 200A and 1,500V. The connectors use a red variant for the positive terminal and a black variant for the negative, similar to a car battery.

TE Connectivity's DYNAMIC D8000 Pluggable Connectors feature an audible locking system and crimping contact design. The lock design ensures safe locking while the crimping contacts save assembly time. The connectors can carry currents as high as 100A per pin for wire-to-wire (WTW) and 90A for wire-to-board (WTB). These connectors are ideal for battery test equipment, battery management systems, factory automation, and robotics.

Tech Tuesdays Takeaway

Connectors come in all shapes and sizes and are designed for diverse uses. The traditional uses are expanding, but EV and plug-in hybrid industries are creating a new wave of connections that are changing the market. Design engineers must be aware of the connectors and contacts to keep the power flowing safely and efficiently in their projects.



« Back


Tommy Cummings is a freelance writer/editor based in Texas. He's had a journalism career that has spanned more than 40 years. He contributes to Texas Monthly and Oklahoma Today magazines. He's also worked at The Dallas Morning News, Fort Worth Star-Telegram, San Francisco Chronicle, and others. Tommy covered the dot-com boom in Silicon Valley and has been a digital content and audience engagement editor at news outlets. Tommy worked at Mouser Electronics from 2018 to 2021 as a technical content and product content specialist.


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos