Advantech’s Rugged MIO-5271 SBCs Using 4th Generation Intel Cores Now at Mouser
November 20, 2014 - Mouser Electronics, Inc. is now stocking the MIO‑5271 Compact Single Board Computer (SBC) from Advantech. The MIO‑5271 is a fanless 3.5‑inch SBC that uses an optimized thermal design based on 4th generation Intel® cores. Advantech SBCs support Multiple I/O (MIO) and networking options as well as high resolution audio and HD video. These SBCs target industrial computing applications and are especially suited for harsh environments.
The Advantech MIO‑5271 Compact Single Board Computers, available from Mouser Electronics, give developers a choice of either a 1.9GHz Intel Core i5‑4300U or a 1.6GHz Intel Celeron 2980U. This allows the MIO‑5271 SBC to deliver the appropriate computational performance while also providing energy efficient behavior for targeted applications. The Advantech MIO‑5271 SBCs support up to 8GBytes of DDR3L DRAM in a single 204-pin SODIMM slot. Two SATA ports are available for hard drive expansion. A user switch allows configuration for either one mSATA port or one miniPCI port. Typical power consumption is about 4.6 Watts.
The MIO‑5271 SBC supports many networking and connectivity options which include two USB 2.0 and two USB 3.0 ports, two Industrial Gigabit Ethernet ports, and up to up to four RS‑232/422/485 ports with ESD protection. A Realtek ALC888S, High Definition Audio codec is supported with Line-in, Line out, and Mic-in connectors. Multiple video‑out options are available including a VGA port and an HDMI/DisplayPort connector.
Advantech 3.5" MI/O-Compact SBCs target wide temperature applications and can operate in 0 to 60°C (0 to 140°F) environments. Advantech's built-in iManager is an intelligent self-monitoring agent with software and hardware control functions including intelligent resource control, system protection and restore, and automatic system bootup and/or recovery in critical conditions.
To learn more, visit: http://www.mouser.com/new/advantech/advantech-mio-5271/ .
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Advantech is a leader in providing trusted, innovative embedded and automation products and solutions. The company offers comprehensive system integration, hardware and software, customer-centric design services, and global logistics support, all backed by industry-leading front- and back-office e-business solutions. Advantech is an innovator and cooperates closely with partners to help provide complete solutions for a wide array of applications across a diverse range of industries.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.