Costa Rica - Marcar Costa Rica

Términos internacionales de comercio (Incoterms):FCA (punto de envío)
Los costos de aranceles, aduana e impuestos se cobrarán en el momento de la entrega.

Confirme su elección de moneda:

Colón costarricense
Solo se aceptan pagos con tarjetas de crédito, excepto American Express

Dólares estadounidenses
Se encuentran disponibles todas las opciones de pago

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Buying From Independents Carries Problems and Risks Chuck Amsden

Last week I had a prime tell us they preferred to buy a part through an independent rather than directly from Mouser, an authorized distributor.

I’ve been told this is for the convenience of the prime. They want to keep their suppler base low and they don’t have an account with Mouser. So they add an extra link to the chain by having the independent buy it from us and then the independent turns around and brokers it to the prime.

Does this mean AS5553A clause 4.1.3 b ”Specify a preference to procure directly from OCMs or authorized suppliers…” lacks teeth? Is it time to have a clause in AS5553 that says “Procure parts from OCMs and Authorized Suppliers when parts are still available from these sources.”?

What customers need to remember is that authorized distributors will not guarantee traceability though a non-authorized distributor. We also will not transfer warranty or support failure analysis though a non-authorized distributor. Many distribution agreements with manufacturers prohibit the sale of their products to non-authorized distributors.

If the parts are available in authorized distribution, they should be purchased within authorized distribution.



« Back


Chuck AmsdenChuck Amsden is the former Vice President of Quality at Mouser Electronics. Amsden joined Mouser in 2003 and helped lead the company to obtain ANS9120A/ISO9001:2008 and ANSI/ESD S20.202007 certifications. Amsden was a contributing member of three SAE G-19 committees, working on standards for mitigating counterfeits in the electronic components supply chain. He also chaired a committee in the Electronic Components Industry Association (ECIA) that developed methods of traceability within authorized distribution and served on the ECIA Certification Task Force focused on mitigating counterfeits.


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos