Costa Rica - Marcar Costa Rica

Términos internacionales de comercio (Incoterms):FCA (punto de envío)
Los costos de aranceles, aduana e impuestos se cobrarán en el momento de la entrega.

Confirme su elección de moneda:

Colón costarricense
Solo se aceptan pagos con tarjetas de crédito, excepto American Express

Dólares estadounidenses
Se encuentran disponibles todas las opciones de pago

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: From Blueprint to Reality: Smart and Efficient Net-Zero Carbon Home Building Rudy Ramos

New Tech Tuesdays

Join Rudy Ramos for a weekly look at all things interesting, new, and noteworthy for design engineers.

The world is witnessing a paradigm shift in home building design, driven by the urgent need to combat climate change. Net-zero carbon home building has emerged as a revolutionary approach that combines sustainability, energy efficiency, and smart technologies. This article explores the progress made in smart and efficient home building design with a net-zero carbon approach, highlighting the transformative impact on the environment and homeowners. From integrating renewable energy systems to leveraging data analytics for energy optimization, the advancements in this field are reshaping how we conceive and construct homes.

Before delving into the subject, it is important to establish a clear understanding of the terms commonly associated with contemporary home building. Let's define some key concepts and guidelines for constructing such a home.

  • Renewable energy refers to energy sources derived from naturally replenishing resources like solar, wind, hydroelectric, geothermal, and biomass. These sources are sustainable and have minimal environmental impact compared to finite fossil fuels.
  • Net-zero carbon, also known as carbon neutrality, describes achieving a balance between carbon dioxide emissions produced and removed or offset from the atmosphere. In the context of home building, a net-zero carbon home minimizes its carbon footprint through energy efficiency, renewable energy integration, and carbon offsetting.
  • Data analytics for energy optimization involves collecting, analyzing, and interpreting data related to a building's energy consumption, performance, and efficiency. By leveraging advanced technologies, such as algorithms and smart systems, data analytics provides insights to optimize energy management decisions and enhance overall building performance.
  • Smart home describes a residence equipped with interconnected Internet of Things (IoT) devices and systems that can be controlled, automated, and monitored remotely through a network, typically via internet connectivity. These devices enable homeowners to manage and optimize various aspects of their homes, including lighting; heating, ventilation, and air conditioning (HVAC); security; and entertainment, for enhanced convenience, energy efficiency, and comfort.

Net-Zero Carbon Home Building

Net-zero carbon home building involves integrating various technologies and systems along with good building practices. Whenever possible, implementing a building-design strategy that uses passive natural ventilation combined with proper building orientation that helps maximize natural lighting and reduces the need for artificial heating and cooling is preferred and yields that most energy-efficient home.

However, this is not always possible or practical, so the energy savings need to come from the home’s building materials, technology, and systems. For instance, a designer may opt to use high levels of insulation and install windows and doors with a high R-value. Using eco-friendly, low-impact, sustainable building materials such as recycled or locally sourced materials will help reduce the home’s overall carbon footprint. Installing energy-efficient appliances and properly sized energy-efficient HVAC systems that optimize energy usage and provide comfortable indoor conditions are key to minimizing the home’s energy consumption.

Furthermore, incorporating solar panels, wind turbines, or geothermal systems to generate clean energy onsite is vital for achieving a net-zero carbon home. Using advanced automation and control systems to monitor and manage energy consumption, optimize usage, and enhance efficiency, along with data analytics tools that track energy usage and identify areas for improvement, are essential steps for realizing the vision of a carbon-neutral home.

Not to be forgotten is the home’s water efficiency. It is also a very important aspect that needs to be considered during the planning stages of the home-building process. By incorporating water-saving fixtures, rainwater harvesting systems, and efficient irrigation methods, the home’s overall water consumption will be reduced and further promote the home’s sustainability and limit dependency on traditional water sources.

Lastly, educating the homeowners about energy-saving practices and encouraging active participation in energy conservation efforts can go a long way towards the goal of achieving a net-zero carbon home.

Net-Zero Carbon Home Building Resources

It's important to note that these key concepts and guidelines are general in nature. The specific implementation and requirements for building a smart, efficient, net-zero carbon home will vary based on individual circumstances, preferences, resources, location, and the level of integration of all the different systems and technologies. There is no one best way to build such a home, but understanding key terms and following some guidelines will lay the foundation for exploring the evolving world of contemporary home building and its innovative approaches to sustainability, efficiency, and enhanced living.

Organizations like the Leadership in Energy and Environmental Design (LEED), the International Living Future Institute (ILFI), the Building Research Establishment Environmental Assessment Methodology (BREEAM), and many others provide valuable resources, certifications, and guidance for sustainable building practices, each with their own specific focus and approach to sustainability. These organizations and programs encourage sustainable practices in design, construction, and operation for single-family homes, multifamily buildings, and residential developments, and consider aspects like energy efficiency, water conservation, indoor air quality, sustainable materials, and site selection. Typical certification involves documentation, verification, and performance testing. Certified buildings benefit the environment, provide energy savings, and improve the comfort of its residents.

Innovative Products for Energy Efficiency

A variety of novel, cutting-edge products are currently present in the market. While some are still in development and unavailable for purchase, others leverage longstanding concepts integrated with state-of-the-art technology, resulting in highly efficient energy-saving solutions. Seeing these innovative and legacy products shape the future of home construction is truly exciting.

Hydropanels make, store, and dispense clean, mineralized water using solar panels that incorporate multiple technologies to produce renewable water using the power of the sun to extract clean, pollutant-free drinking water from the air. The collected water is then mineralized for ideal composition and taste, making premium-quality drinking water a readily available resource.

Hydropanels exemplify an ingenious solution that harnesses the power of the sun to produce, store, and distribute clean, mineralized water. By combining solar panels with advanced technologies, these innovative systems represent new possibilities for energy efficiency. Hydropanels enable premium quality drinking water to be easily accessible and convenient, eliminating the need for bottled water.

SolarWindow touts electricity-generating liquid coatings and processes that use LiquidElectricity® technology and are transparent, ultra-lightweight glass and flexible plastics that work in natural and artificial light. This product is currently under development and not commercially available for sale, but it is interesting to see where the outer fringes of sustainable energy-generating products are going.

WaterFurnace offers residential geothermal energy systems for heating and cooling using geothermal heat pumps. By harnessing the free, renewable solar energy stored in the ground, WaterFurnace heat pumps provide a natural and cost-effective way to significantly reduce energy bills. Unlike the previous two futuristic innovative products, WaterFurnace’s heat pump technology has been around since 1983 and has systems installed in all 50 states and countries worldwide. By integrating cutting-edge technologies into their core business, WaterFurnace systems represent an innovative, clean, and sustainable energy solution that combine superior engineering and unmatched quality, making them among the most efficient heating and cooling residential and commercial systems available today.

ecobee and Nest HVAC thermostats optimize energy consumption in buildings by learning the occupants' preferences and adjusting the temperature settings accordingly. These ENERGY STAR certified self-learning smart devices can be easily integrated into a home’s ecosystem and allow for the convenience of remote control via mobile devices.

Featured Products

This week’s New Tech Tuesday highlights industry-leading products from Amphenol Advanced Sensors and Advantech. These devices represent years of engineering and manufacturing expertise and a total commitment to quality and reliability by these suppliers.

Amphenol Advanced Sensors’ Telaire T6793 Carbon Dioxide (CO2) Sensor Series are compact, reliable, and accurate CO2 sensor modules designed for optimal demand control, indoor air quality management, and energy savings. The T6793 and T6793-5K sensors have a measurement range of 0-2000ppm and 0-5000ppm, respectively, and are non-dispersive infrared (NDIR) diffusion sampling sensors that meet the rigorous Title 24 accuracy standards set by the California energy code. These sensors operate with an accuracy rating of ±45ppm +3% in the 400-5000ppm range. Their innovative features include:

  • Cost-effective gas-sensing solutions
  • Telaire ABC Logic software for eliminating most calibration needs
  • Signal updates every five seconds
  • Seamless interaction with other microprocessor devices

Their dependable design ensures easy integration and operation within various environments. With measurements updated every five seconds and no calibration needed for most applications, these sensors promise simplicity, efficiency, and precision in one compact package. Integrating a Telaire T6793 sensor can deliver an added intelligence layer to any net-zero carbon home building blueprint, rendering it a game changer in maintaining optimal indoor air quality, maximizing energy savings, and proving that intelligent building design and sustainability can coexist in harmony.

The Advantech ECU-150 High-Performance Quad Core IoT Gateway is an NXP i.MX8M with 2GB of LPDDR4 memory. The ECU-150 features an open platform design with two RS-232/485 serial ports, two 10/100/1000 Ethernet ports, and an expansion Mini-PCIe with M.2 slots for integrating Wi-Fi/4G/5G communication modules. These Advantech intelligent communication gateways are Arm®-based robust platforms with wireless and Ethernet communication, as well as multiple protocol support. Advantech's communication gateways are designed to optimize data acquisition and transmission. In the broad fields of IoT and Industrial IoT, the objective is to leverage data analytics for improved service and reduced operational costs. The ECU-150 presents an inventive solution that accomplishes precisely that by facilitating connectivity across infrastructure, monitoring devices, and analyzing energy usage.

Advantech's ECU-150 gateways address the increasing demand for a reliable, durable, and user-friendly approach to extracting, gathering, and handling data from applications such as solar power, electricity monitoring, and factory automation. These applications require extensive data collection, cloud-based functionality, and video monitoring solutions. Design engineers can rely on the flexibility of these gateways to optimize their residential and commercial applications, gaining valuable usage insights and leveraging intelligence through thorough data analysis.

Tuesday’s Takeaway

In the quest for a sustainable future, the development of smart and efficient net-zero carbon home construction provides cause for satisfaction. The building sector is starting to implement innovative practices like energy-efficient technologies and renewable energy integration into the home building process, specifically aimed at helping to reduce the carbon footprint of our dwellings. Due to growing market demand, net-zero carbon homes and buildings are increasingly becoming attainable and appealing to homeowners and businesses alike. However, achieving widespread adoption and scalability calls for collective efforts from buyers, builders, and product and material manufacturers, as well as continuous innovation and supportive regulations and policies. By incorporating products like those showcased this week from Amphenol Advanced Sensors and Advantech, our way of building and living can be transformed, resulting in a healthier, eco-friendlier, and more sustainable future.



« Back


Rudy RamosRudy Ramos brings 35+ years of expertise in advanced electromechanical systems, robotics, pneumatics, vacuum systems, high voltage, semiconductor manufacturing, military hardware, and project management. Rudy has authored technical articles appearing in engineering websites and holds a BS in Technical Management and an MBA with a concentration in Project Management. Prior to Mouser, Rudy worked for National Semiconductor and Texas Instruments..


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos