Costa Rica - Marcar Costa Rica

Términos internacionales de comercio (Incoterms):FCA (punto de envío)
Los costos de aranceles, aduana e impuestos se cobrarán en el momento de la entrega.

Confirme su elección de moneda:

Colón costarricense
Solo se aceptan pagos con tarjetas de crédito, excepto American Express

Dólares estadounidenses
Se encuentran disponibles todas las opciones de pago

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: Tri-Radio Tech Upgrades Smart Home Connectivity Mouser Technical Content Staff

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

Connectivity is paramount in the rapidly evolving world of smart homes and the Internet of Things (IoT). To meet these needs, the NXP RW612 Tri-Radio device stands out by integrating Wi-Fi 6, Bluetooth® Low Energy, and 802.15.4 connectivity options, offering enhanced speed, capacity, and security. In this week’s New Tech Tuesdays, we take a closer look at these connectivity advancements.

Wi-Fi 6: Enhanced Speed and Capacity

Wi-Fi 6 has been a game-changer in wireless connectivity, providing faster speeds and greater capacity. This technology allows multiple devices to connect simultaneously without compromising performance. For smart homes, this means better coverage and stronger connections for devices throughout the home, including outdoor security cameras.

For security systems that rely on real-time, high-definition video streaming, Wi-Fi 6 helps enable clearer, more reliable video feeds, which is crucial for today’s smart homes to monitor and respond to security incidents.

Wi-Fi 6 also supports advanced security protocols like WPA3 encryption, offering stronger protection against network threats. This is particularly important for smart home devices that handle sensitive personal data and home access.

Bluetooth Low Energy: Low Power Consumption

Bluetooth Low Energy is designed for energy-efficient communication, making it ideal for battery-powered devices. It excels in short-range communication, which is perfect for devices such as smart locks and sensors. Additionally, this communication technology brings intermittent data transfer and compatibility to devices in and around the smart home.

  • Intermittent data transfer: Bluetooth Low Energy is suitable for applications requiring intermittent data transfer, such as health monitoring devices and wearables. It ensures that data is transmitted efficiently without draining the battery.
  • Compatibility: Bluetooth Low Energy is widely supported by mobile operating systems, ensuring seamless integration with smartphones and tablets. This makes it easy for users to control and monitor their smart home devices from their personal mobile devices.

802.15.4: Multi-Protocol Support

The NXP RW612 Wireless MCU’s versatile connectivity options make it suitable for widespread adoption in smart homes. IEEE 802.15.4 enables this versatile connectivity by supporting Thread and Zigbee®, protocols that are especially relevant to the Matter ecosystem.

Thread can create a mesh network environment that operates with lower latency, making it suitable for applications requiring rapid responses and reliable data transmission. In the Matter ecosystem, Thread’s mesh network can increase the range of communication and reliability by adding multiple nodes that can be used in case any single point fails. Zigbee provides low power consumption and higher maturity with a well-established ecosystem and a wide range of existing users. The Zigbee support on the RW612 enables compatibility to those already-existing users.

The Newest Products for Your Newest Designs®

The NXP Semiconductors FRDM-RW612 Wireless MCU development board (Figure 1) is designed for rapid prototyping with the RW61x family of Wi-Fi 6, Bluetooth Low Energy, and 802.15.4 Tri-Radio microcontrollers. This compact and scalable board offers easy access to the microcontroller’s I/Os, peripherals, integrated serial interfaces, and external flash memory. It includes an onboard MCU-Link debugger based on the LPC55S69 MCU, making it a versatile tool for developers working on wireless connectivity projects.

Figure 1: NXP Semiconductors FRDM-RW612 development board. (Source: Mouser Electronics)

The FRDM-RW612 board simplifies the development process for smart home devices, industrial automation, and other applications requiring robust wireless communication. With features like dual-band Wi-Fi 6, Bluetooth Low Energy, and 802.15.4 support for Zigbee and Thread, this board ensures reliable and efficient connectivity. Additionally, it comes with expansion options such as Arduino headers and Pmod connectors, allowing users to easily integrate additional components and sensors.

Tuesday’s Takeaway

The NXP RW612 is revolutionizing modern connectivity with its Tri-Radio technology. By integrating Wi-Fi 6, Bluetooth Low Energy, and 802.15.4, it enhances speed, capacity, security, and efficiency in modern devices. Whether for high-definition streaming, energy-efficient communication, or seamless device interaction, the NXP RW612 is a cornerstone of the smart home and IoT landscape.



« Back


Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos