Términos internacionales de comercio (Incoterms):FCA (punto de envío) Los costos de aranceles, aduana e impuestos se cobrarán en el momento de la entrega.
Confirme su elección de moneda:
Colón costarricense Solo se aceptan pagos con tarjetas de crédito, excepto American Express
Dólares estadounidenses Se encuentran disponibles todas las opciones de pago
Vishay Exterior LED Fog Lighting Solutions address the automotive front where lighting provides a stable input voltage for the switched-mode current regulator, an essential tool. First, the battery voltage has to be stabilized with a Buck-Boost to provide a stable input voltage to the following multiple Buck converter stages. Depending on LED-string solutions, the total current defines the power level of various buck stages. The main buck-boost has to have the full power level for the complete lighting control unit. The efficiency of buck-converters depends on synchronous or non-synchronous topology. The light engine is also a feedback loop for LED-string current control and is quite essential.